AXIS#.TUNING.TARGETBANDWIDTH

Description

AXIS#.TUNING.TARGETBANDWIDTH displays the target bandwidth calculated by the most recent QuickTune procedure since the drive booted up.

  • If AXIS#.TUNING.USERBANDWIDTH is set to 0, AXIS#.TUNING.BANDWIDTH will be set to the most recently calculated AXIS#.TUNING.TARGETBANDWIDTH at the end of QuickTune procedure.

    This value is updated with every QuickTune procedure regardless of AXIS#.TUNING.USERBANDWIDTH. If the target bandwidth cannot be calculated, AXIS#.TUNING.TARGETBANDWIDTH will be set to 0.

Versions

Action Version Notes
Implemented 02-12-02-000 

-

General Information

Type Read Only
Units Hz
Range N/A
Default Value N/A
Data Type Double
See Also AXIS#.TUNING.QUICKTUNE.START
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.TARGETBANDWIDTH

5021h

07h

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5041

1

5041 (0x13b1)

AXIS1.TUNING.TARGETBANDWIDTH

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TUNING.TARGETBANDWIDTH

5041

Float

Read Only

-